¿Listo para llevar su moldeo por inyección al siguiente nivel? Descubra la última tecnología de moldeo por inyección eléctrica de ROBOSHOT, diseñada para ofrecer una precisión, una velocidad y una eficiencia energética excepcionales. Explore el control CNC avanzado con una interfaz táctil intuitiva, supervisión energética integrada y funciones diseñadas para maximizar la eficiencia de la producción. Con un hardware robusto diseñado para garantizar una fiabilidad a largo plazo, ROBOSHOT le ayuda a lograr una calidad constante y un alto rendimiento en cada ciclo.
Služba Nitra, a Slovakian manufacturer supplying mostly to the automotive sector, has transformed its production through extensive automation in the shape of FANUC CNC injection moulding machines and high-performance industrial robots. By upgrading its assembly lines and moulding shop, the company has significantly increased productivity while cutting energy consumption and reducing error rates. The result is a highly efficient, reliable and sustainable manufacturing environment supporting major auto OEMs and tier-one suppliers.
All growing manufacturers need a reliable technology partner with innovative machines and solutions that can underpin success in the globally competitive market. Able to provide suitable testimony is Germany-based AKO Kunststoffe GmbH, a fourth-generation family-run injection moulding business that relies on around 30 FANUC ROBOSHOT all-electric injection moulding machines, including eight automated with FANUC industrial robots.
Although electricity prices levelled off across 2023 and 2024 following huge spikes in 2020 and 2022, they are still significantly higher than pre-pandemic levels, with many experts predicting they may remain high for the rest of this decade and potentially beyond. The way for beleaguered manufacturers to fight back is to invest in energy-efficient machinery, just like the FANUC ROBOSHOT injection moulding machine.
Los clientes pueden esperar de la máquina de moldeo por inyección totalmente eléctrica ROBOSHOT de FANUC una alta eficiencia de producción, bajos costes energéticos y bajas emisiones de ruido, junto con un gran servicio y soporte técnico.