J. SCHNEEBERGER Maschinen AG

Automatización modular de CNC y robots con una plataforma común

El fabricante de rectificadoras CNC SCHNEEBERGER Maschinen AG eligió a FANUC por su reputación mundial, sus productos duraderos y su red de asistencia. FANUC proporcionó una solución integral con CNC, robots y motores, permitiendo una comunicación perfecta. La adopción del último CNC 31𝑖-B de FANUC mejoró el diagnóstico y la calidad del rectificado de herramientas.
Case Study Schneeberger about taking advantage of  a single control platform for CNC and robot, with the industrial PC providing user-friendly data exchange.

Key Insights from Task to Result

Task

CNC tool-grinding machine manufacturer J. SCHNEEBERGER Maschinen AG wanted to find an automation solutions specialist that could control separate CNC and robot technologies using a common platform. The supplier would also have to provide worldwide support over the lifetime of the machines. 

Solution

SCHNEEBERGER selected FANUC based on the company’s worldwide reputation, durable products and global support network. FANUC supplies SCHNEEBERGER with an optimal combination of 31𝑖-B series CNC, PANEL 𝑖H Pro industrial PC, SCARA SR-12𝑖A and LR Mate 200𝑖D robots, and linear and torque motors. FANUC I/O Link𝑖 facilitates serial communications between CNC and robot.

Result

SCHNEEBERGER precision tool grinders take advantage of a single control platform for both CNC and robot, with the industrial PC providing user-friendly data exchange. Furthermore, the use of FANUC motors has brought a clear improvement in tool-grinding quality and precision. Over the past year, adoption of the latest FANUC 31𝑖-B CNC has introduced even greater diagnostics capabilities.

About J. SCHNEEBERGER Maschinen AG

Success story Schneeberger about taking advantage of  a single control platform for CNC and robot, with the industrial PC providing user-friendly data exchange.
Success story Schneeberger about taking advantage of  a single control platform for CNC and robot, with the industrial PC providing user-friendly data exchange. FANUC Switzerland

Based in Roggwil, around 40km west of Zürich, Switzerland, SCHNEEBERGER is a family-owned manufacturer of CNC precision tool-grinding machines. Founded in 1923, the company has around 180 employees worldwide and customers in practically every developed country. SCHNEEBERGER’s dense network of service facilities local to its customers support the company’s activities in a plethora of industries, including automotive, aerospace and energy.

FIND OUT MORE ABOUT Schneeberger

The Right Tools for the Job

“Our CNC precision tool grinders need to meet a number of important criteria,” states Hartmut Rühl, Head of Software Development at SCHNEEBERGER. “Firstly, they must process hard cutting-tool materials such as carbide, HSS [high-speed steel] and ceramics. Our machines must also achieve ultra-high precision, in the micron range, while another prerequisite is ensuring optimal surface quality.”

Around 30 years ago, SCHNEEBERGER began searching for an industrial control that was highly flexible, precise and dynamic, and able to interpolate at least five axes simultaneously. For communication with the operator, a user-friendly interface was also essential. 

Success story Schneeberger about taking advantage of  a single control platform for CNC and robot, with the industrial PC providing user-friendly data exchange.
Success story Schneeberger about taking advantage of  a single control platform for CNC and robot, with the industrial PC providing user-friendly data exchange. FANUC Switzerland
Testimonios

Hartmut Rühl

Head of Software Development at SCHNEEBERGER

The solution supplied to SCHNEEBERGER today is based on a FANUC 31𝑖-B CNC with FANUC PANEL 𝑖H Pro industrial PC. Thanks to the use of FANUC I/O Link𝑖, the CNC and FANUC robots communicate via a single control platform. 

“For us, connection between the robot and CNC is a great advantage,” declares Antonio Grasso, Head of Electronic Development at SCHNEEBERGER. “It means that our users can monitor two completely different systems with one control. What’s more, our adoption of the latest 31-𝑖B control means we now have a CNC with even better diagnostics capabilities, thus enhancing machine reliability.”

FANUC provided a comprehensive solution, combining CNC, robots, and motors with seamless communication, to the CNC tool‑grinding machine manufacturer SCHNEEBERGER Maschinen AG. FANUC's 31i-B CNC improved diagnostics and enhanced tool-grinding quality.

As another benefit, SCHNEEBERGER has been using FANUC linear and torque motors since the beginning of 2000. These motors help deliver the short, fast oscillating motion of SCHNEEBERGER machines as part of the tool-grinding process. According to Grasso, “this has brought a clear improvement in grinding quality and tool precision”.

Today, SCHNEEBERGER is a near-exclusive user of FANUC products: robots, CNCs and motors.

“FANUC has proven to be a very reliable and competent partner for us over the years,” concludes Rühl.

Automated CNC grinding with FANUC Robot LR Mate 200iD at CNC tool‑grinding machine manufacturer SCHNEEBERGER Maschinen AG.

Inspírese

FANUC Success with Robots, ROBOSHOT and ROBODRILL - Erkul Cosmetics in Turkey benefits from FANUC's variety of products in order to improve quality and efficiency.

FANUC Case Studies

Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.