Scopri i notevoli risultati ottenuti grazie alle soluzioni di automazione di fabbrica FANUC. Scopri come la nostra tecnologia trasforma i settori industriali e favorisce il successo.
Automated CNC machining cells comprising various machine tools and robots require astute design and integration. So why not simplify the process by turning to the world’s most prominent manufacturer of both CNC machine tools and robots: FANUC. That was precisely the strategy of RADMOT, a major Poland-based provider of machining services when it wanted to implement a new CNC milling cell involving three machining centres and two robots that could run unmanned 24 hours a day, 7 days a week – without any collisions between robots.
What do most contract machining companies consider when looking to reach the next level of efficiency, productivity and reliability? The answer, of course, is automation. For this very reason, Germany-based WU Mechanische Werkstätte GmbH built an automation cell -featuring a FANUC industrial robot - for loading and unloading one of its own machine tools. Two years later, a visitor liked the concept so much he asked WU to build him one. This marked the beginning of an additional revenue stream based on the design and build of automation cells featuring high-performance industrial robots from FANUC.
In the manufacture of popular household appliances such as coffee grinders, a number of prerequisites determine production success. For instance, only clearly structured, efficient and target-orientated processes will result in the required levels of production reliability. Achieving this ambition becomes significantly more realistic using automation, as market leader Eugster/Frismag AG can testify following its adoption of 14 FANUC LR Mate industrial robots and FANUC ZDT (Zero Down Time), which now enable the continuous automated assembly of a coffee grinder every 7 seconds.
In a fast-moving fresh-food distribution plant, efficiency through automated packing operations is paramount to keep pace with demand. As a by-product of this approach, robot adopters also gain from less physical strain for employees, gentler handling of delicate produce like fruit and vegetables, and more a uniform and repeatable process. Among the latest factories to benefit from all this added value is the Bätterkinden, Switzerland facility of major food distributor Inoverde, where carrot filling, packing and palletising operations are benefiting from the introduction of three FANUC industrial robots.
Lo sviluppo di una nuova versione di un processo antico come la tornitura richiede livelli sovrumani di creatività e innovazione. Inoltre, convertire queste nuove visioni e concetti di macchine in realtà richiede una tecnologia di controllo estremamente avanzata. Con questo pensiero in mente, il costruttore di macchine utensili FFG Werke sapeva esattamente a chi rivolgersi per ottenere un sistema CNC con le capacità e le prestazioni necessarie per completare il suo nuovo e rivoluzionario centro di tornitura verticale: FANUC.
Esplora e scarica immagini, video e documenti ufficiali FANUC dalla nostra Libreria multimediale.
Metteti in contatto con i nostri specialisti in PR e comunicazione di FANUC Europe