Media data stream portal

Actualités et médias

Les dernières nouvelles, les études de cas et les événements à venir du premier fournisseur mondial d'automatisation industrielle.

Études de cas

 

Découvrez des réalisations remarquables alimentées par les solutions d'automatisation d'usine de FANUC. Voyez comment notre technologie transforme les industries et propulse le succès.

Images WU GmbH Case study featuring and LR-10iA/10 and ROBODRILL.
WU Mechanische Werkstätte GmbH

Success of FANUC Robot Cell Leads to New Revenue Stream

What do most contract machining companies consider when looking to reach the next level of efficiency, productivity and reliability? The answer, of course, is automation. For this very reason, Germany-based WU Mechanische Werkstätte GmbH built an automation cell -featuring a FANUC industrial robot - for loading and unloading one of its own machine tools. Two years later, a visitor liked the concept so much he asked WU to build him one. This marked the beginning of an additional revenue stream based on the design and build of automation cells featuring high-performance industrial robots from FANUC.

Images Eugster/Frismag Case Study. Assembling of coffee grinders with LR Mate 200iD/7L and handling with M-20iD/25 in combination with ZDT.
Eugster/Frismag

Fully Automated Assembly of Coffee Grinders

In the manufacture of popular household appliances such as coffee grinders, a number of prerequisites determine production success. For instance, only clearly structured, efficient and target-orientated processes will result in the required levels of production reliability. Achieving this ambition becomes significantly more realistic using automation, as market leader Eugster/Frismag AG can testify following its adoption of 14 FANUC LR Mate industrial robots and FANUC ZDT (Zero Down Time), which now enable the continuous automated assembly of a coffee grinder every 7 seconds.

Images Inoverde Case Study. Picking, Packing, Palletising of carrots with M-20iD/25, M-20iD/35, and M-710iC/50 and DCS.
Inoverde

Trio of FANUC Robots Boost Packing Efficiency at Inoverde

In a fast-moving fresh-food distribution plant, efficiency through automated packing operations is paramount to keep pace with demand. As a by-product of this approach, robot adopters also gain from less physical strain for employees, gentler handling of delicate produce like fruit and vegetables, and more a uniform and repeatable process. Among the latest factories to benefit from all this added value is the Bätterkinden, Switzerland facility of major food distributor Inoverde, where carrot filling, packing and palletising operations are benefiting from the introduction of three FANUC industrial robots.

Images FFG Werke case study: Pick-up vertical turning machines for top production quality featuring CNC Series 31iB Plus
FFG Werke

La CNC FANUC multi-capacités donne une nouvelle dimension au tournage vertical

Le développement d'une nouvelle approche d'un processus séculaire tel que le tournage requiert des niveaux surhumains de créativité et d'innovation. De plus, la concrétisation de ces nouvelles visions et concepts de machines nécessite une technologie de commande extrêmement avancée. Dans cette optique, le constructeur de machines-outils FFG Werke savait exactement vers qui se tourner pour trouver un système CNC doté des capacités et des performances nécessaires pour compléter son nouveau centre d'usinage vertical révolutionnaire : FANUC.

Bern, FANUC, Münzen, Münzprägerei, Swissmint
Images Swissmint case study
Swissmint

Les robots FANUC automatisent la production de pièces de monnaie chez Swissmint

Automatiser l'ensemble du processus de frappe de la monnaie, depuis les pièces individuelles jusqu'aux boîtes palettisées finies, n'est pas une mince affaire. C'est pourtant la tâche à laquelle a été confronté Swissmint, l'Hôtel des monnaies de Suisse. Pour faire de ce concept complexe une réalité, Swissmint déploie des robots FANUC haute performance dans des tâches telles que le pick and place, l'assemblage de boîtes et la palettisation.