Skip to main content
FBL success story featuring handling of kegs.

Roboti za paletiranje FANUC

Družba FANUC ima na voljo najzmogljivejšo paleto robotov za paletiranje, ki izpolnjujejo vse vaše zahteve glede koristnega tovora. Ne glede na to, ali zlagate celotno plast ali posamezne škatle, vreče, vedra ali bobne, koboti in roboti FANUC zagotavljajo hitro, stabilno in zanesljivo rešitev za avtomatizacijo.

Prenesi za dodatne informacije

Dostop do bistvenih tehničnih specifikacij in dragocenih informacij o naših izdelkih prek naših dokumentov za prenos, ki vam bodo pomagali sprejeti prave odločitve in kar najbolje izkoristiti izdelke FANUC.

Navdihnite se

Navdihujte se pri uspehu drugih

The milling company Lindmühle uses a FANUC M-710iC six-axis articulated arm robot for an automated solution where 5 to 25 kg bags of flour are stacked automatically and each bag is weighed. Not only has the FANUC robot relieved workers at Lindmühle from the physical strain of lifting 5 to 25 kg flour bags onto pallets, but it has also helped the company achieve a 50% increase in its palletising capacity.
Lindmühle

Robot FANUC poveča zmogljivost paletiranja v tovarni moke

Prevzemanje bremen pri dvigovanju težkih tovorov je klasična aplikacija za industrijske robote. Vendar pa uporaba robotov pri nalogah dvigovanja ne pomeni le fizične razbremenitve delavcev, temveč lahko poveča tudi prepustnost, tudi če je prostor omejen. Primer je proizvajalec moke Lindmühle, kjer je programska oprema za simulacijo FANUC izpostavila optimalnega robota za razpoložljiv delovni prostor.

Robotic Palletizing and Stretch Wrapping Line with FANUC Robot M-410iC/185.
Keramik

FANUC Robots Extend the Benefits of Stretch Hood System

Keramik Makina, a FANUC system integrator, combined palletising and shrink hood systems with FANUC robots to form powerful end-of-line solutions at the paint factory of Polisan Kansai in Türkiye.

M-710iD/50 palletising bottles.
Brunos

FANUC Robot Ends Packaging Bottleneck at Food Factory

When implementing improvements to a bottleneck process the common outcome is the emergence of a new bottleneck elsewhere in the factory. Whereas in years gone by this situation would necessitate the recruitment of more labour, automation has today become industry’s go-to solution for bottlenecks. Just ask Brunos, a leading producer of salad dressings, which knows all about the benefits that a robot can bring.