FANUC Solutions Provide Common Thread at Screw-Cutting Specialist
Moving from labour-based to automated production operations can sometimes appear daunting. And yet, with the right technology partner on-board, processes such as automated machining and assembly can come to realisation with relative ease, instantly delivering new levels of productivity and reliability.
FANUC products ensure enhanced productivity, repeatability and cost-efficiency.
FANUC ROBOCUT wire EDM running reliably for more than 30 years.
Extremely low failure rate across the entire suite of FANUC products on site.
Reliable FANUC customer support.
Insights
Company
Story
Products
Insights
Key Insights from Task to Result
Task
Joseph Martin recognises that its investments and innovations allow it to meet the industrial challenges of tomorrow. However, a successful outcome of this premise relies upon the astute selection of optimal technologies. In the 1990s, the company wanted to commence a programme of investment that would set it on a course of automated production in support of growing customer demand.
Solution
In 1990, Joseph Martin invested in its first FANUC machine, a ROBOCUT wire EDM, followed soon after by FANUC ROBODRILL milling machines. Furthermore, Joseph Martin today has numerous FANUC six-axis robots on site performing key assembly and part transfer operations.
Result
Much of Joseph Martin’s production now features FANUC automation, both for machining and assembly operations. Providing enhanced productivity, repeatability and cost-efficiency over many years, the company reports an extremely low failure rate across its entire suite of FANUC products. The company also praises FANUC’s highly reactive and competent service team on the rare occasions it requires support.
Company
Joseph Martin
Joseph Martin is a global leader in the screw-cutting of components for automotive transmission systems. Established in 1946 and located at a 20,000 m2 facility in Vougy, close to Chamonix in the French Alpine region, the company performs high-precision bar turning in the production of key automotive components such as solenoids (which drive clutches and activate gear changes). Also specialising in the manufacture of complete sub-assemblies, Joseph Martin has approximately 200 employees who help generate an annual turnover of around €25 million.
“In 1990 we acquired our first FANUC machine, a ROBOCUT CNC wire EDM, an incredibly reliable product which is still in operation today,” reports Alexandre Pessey, Technical Manager at Joseph Martin. “Through the 1990s we added more CNC machine tools, selecting machines with FANUC control systems, such as Tornos MultiSwiss multi-spindle automatic lathes.”
Today, production at Joseph Martin’s manufacturing facility in Vougy includes modern ROBOCUT wire EDMs, ROBODRILL machining centres and FANUC six-axis robots such as the LR Mate 200𝑖D/7L.
“When we had to automate our own control and assembly machines in 2015, we chose to partner with FANUC for our six-axis robot requirements,” explains Pessey. “We’ve always appreciated the reliability of FANUC products, along with the quality of the company’s aftersales service.”
Alexandre Pessey
Technical Manager
The site of FANUC France in Marnaz happens to be less than 3 km from Joseph Martin’s Vougy headquarters.
“Although we see an extremely low failure rate on the entire FANUC range, we enjoy very good reactivity in the rare event of downtime,” says Pessey. “FANUC’s service and repair team are highly responsive and the company is the only manufacturer in its field to maintain the supply of spare parts throughout the lifetime of its machines.”
While Joseph Martin is fortunate enough to enjoy close proximity to a FANUC facility, FANUC Europe excels in technical support and service, regardless of location. The company has approximately 1,000 people dedicated to customer service and repair activities, providing support for as long as the customer uses FANUC products, without time limitation.
A highly satisfied Pessey concludes: “Today I would recommend FANUC for their customer service, product selection advice, repair service and availability of spare parts.”
Products
Get Behind the Technology: Discover Related Products
Introducing the ROBOCUT 𝛼-C400𝑖C model – the compact match for micro machining. This cutting-edge machine sets new standards in precision and versatility, making it the perfect choice for industr...
With their standard stroke, these machines stand out as the epitome of versatile vertical machining centers. They excel in boosting productivity across various milling and drilling tasks that deman...
The LR Mate 200𝑖D/7L is a versatile 6-axis robot with the longest reach in the LR Mate range at 911 mm. Designed for multi-purpose industrial applications, it combines compactness with extended re...
Elevate your precision machining. Designed for high-speed, precision machinery, FANUC 30𝑖-B Plus is the perfect solution for complex applications involving multiple axes and multipath operations. ...
The 0𝑖-TF Plus is a fundamental CNC system tailored for turning applications, optimally designed to enhance the functionality of standard lathes. This basic yet capable system offers customisable ...
Explore our comprehensive range of factory automation solutions, showcased in detailed case studies, and designed to optimise and streamline any manufacturing process.
Wire EDM (Electrical Discharge Machining) is a precision manufacturing process that uses a thin, electrically charged wire to cut intricate shapes and contours in hard metals and conductive materials. The wire generates a series of rapid electrical discharges, which erode the material with extreme accuracy without applying mechanical force. This non-contact method allows for the production of highly detailed, complex parts with excellent surface finishes, making it essential for industries that require precise machining, such as aerospace, medical, and mould-making.
CNC milling is a machining process that uses computer-controlled rotating cutting tools to remove material from a workpiece to create a desired shape. It is widely used for producing precision parts with complex geometries. The process involves securing the workpiece on a movable table and using various tools to cut, drill, and shape the material based on programmed instructions.
CNC turning is a machining process where a cutting tool removes material from a rotating workpiece to create precise cylindrical shapes. It is ideal for producing parts with complex geometries and tight tolerances. In order to maximise your turning centre or lathe’s output, having a good CNC capable of managing and optimising a whole array of turning processes is essential. In addition to maximising productivity, a good CNC will also provide you with the flexibility to reduce turnaround times on small batches.